Search FAQs
Is the ATV630 (or ATV930) Process drive available with 1 phase input and 3 phase output?
Issue:
Are the Process drives available with single phase input and 3 phase output?
Product Line:
Altivar 630
Altivar 930
Environment:
Application
Cause:
Wants to know if the ATV630 Process drive is offered in 1 phase input 3 phase output.
Resolution:
The ATV630 is approved for some single phase input, 3 phase output applications.
See the current Annex to the Getting Started with Altivar Process ATV600 document below:
https://www.se.com/ww/en/download/document/EAV64300/
This document lists models for 240V and 480V Pump applications.
Note: Do not use ATV630D55M3 and ATV630D75M3 for 1-phase application.
At this time, no ATV900 Process drives are approved for single phase supply. They are designed strictly for 3 phase input power to run a 3 phase motor.
The ATV900 series may be used in conjunction with a 3rd party input bridge from a company like Bonitron (Bonitron Solutions for Schneider Drives) .
Contact Bonitron directly for assistance.
Are the Process drives available with single phase input and 3 phase output?
Product Line:
Altivar 630
Altivar 930
Environment:
Application
Cause:
Wants to know if the ATV630 Process drive is offered in 1 phase input 3 phase output.
Resolution:
The ATV630 is approved for some single phase input, 3 phase output applications.
See the current Annex to the Getting Started with Altivar Process ATV600 document below:
https://www.se.com/ww/en/download/document/EAV64300/
This document lists models for 240V and 480V Pump applications.
Note: Do not use ATV630D55M3 and ATV630D75M3 for 1-phase application.
At this time, no ATV900 Process drives are approved for single phase supply. They are designed strictly for 3 phase input power to run a 3 phase motor.
The ATV900 series may be used in conjunction with a 3rd party input bridge from a company like Bonitron (Bonitron Solutions for Schneider Drives) .
Contact Bonitron directly for assistance.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: