{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Test reports according to NF F or EN / ISO of PM3200
We only have IEC 62053-21, -22 -23; IEC 62052-11 and EC 61557-12 test reports,same is attached (SIMT report for PM3255.pdf). NF F or EN/ISO test reports are not available.

Schneider Electric Saudi Arabia

Attachment(s)
SIMT report for PM3255.pdf [14.79 MB]
UL Yellow cards for plastics.zip [205.11 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.