{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an encoder be used with the ATV600 Series Process Drives?
Issue:
ATV600 Series Process Drive encoder usage

Product Line:
ATV630 ATV650 ATV680 Process Drive

Environment:
All models and serial numbers

Cause:
None

Resolution:
The ATV600 series Process drives do not have the ability to be used with an encoder. The ATV900 series is designed for encoder option modules.

Schneider Electric Saudi Arabia