Search FAQs
Can a reversing contactor be used with an ATS22?
Issue:
Running ATS22 in reverse with a contactor
Product Line:
ALTISTART 22
Environment:
All ATS22 Serial Numbers
Cause:
Need to reverse the motor rotation
Resolution:
Yes, it is possible to use a reversing contactor with ATS22. See attached enclosed ATS22 manual.
Running ATS22 in reverse with a contactor
Product Line:
ALTISTART 22
Environment:
All ATS22 Serial Numbers
Cause:
Need to reverse the motor rotation
Resolution:
Yes, it is possible to use a reversing contactor with ATS22. See attached enclosed ATS22 manual.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: