{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When changing Magelis Screen sizes, do we need to change anything in the application?
Issue:
What changes are needed when we migrate to a different model or series of HMI in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
When you change screen sizes, you are essentially using a new Magelis HMI model in the series. You will need to update the Model Selection in the Target Property Inspector. You should also check that any of the settings in the I/O Manager still apply to the new model. Often times, the COM port layouts can be different and you need to make sure you have the right settings and the right cabling.

Schneider Electric Saudi Arabia