{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the short circuit withstand current for iC60 and C60 MCBs?

We have not tested iC60/C60 for Icw test as per IEC 60947-2 standard. Icw (Rated short-time withstand current) tests are more dedicated to the switch-disconnector ranges (according to IEC60947-3) or Utilization Category B Circuit breakers

Schneider Electric Saudi Arabia