{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the drive motor thermal current (ItH) adjustment range for the ATV61/ATV71 drives?
Issue:
Motor thermal current range for the ATV61/ATV71 drives.

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Can't dial down setting ItH to 0

Resolution:
The range is from 25% to 120% of the drive's rated current.

Schneider Electric Saudi Arabia