Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Video: How do I calibrate the Analog Output (FM) on the ATV212 drive?
Issue:
Scale the Analog Output (FM) on the ATV212 drive.

Product Line:
ATV212
S-Flex

Environment:
All models and serial numbers.

Resolution:
When using voltage (0-10Vdc) connect your load prior to calibration.  When using current (4-20mA) connect the load after calibration.
 
If you want to follow OUTPUT CURRENT (FMSL = 1)
4-20mA (no load)
  1. Set DIP switch FM (SW101) to "I" (left)
  2. Set F692 for 20 (20% of 20mA = 4mA)
  3. Set FMSL to 15 
  4. Go to parameter FM and enter
  5. Connect the current meter to terminals FM and CC
  6. Press the UP and DOWN arrows until meter reads desired 100% (20mA)
  7. Press enter to lock in the scale
  8. Set FMSL = 1 to follow motor current
0-10Vdc (connect the load)
  1. Set DIP switch FM (SW101) to "U" (right)
  2. Set F692 to 0 (0% of 10V = 0V)
  3. Set FMSL to 15
  4. Go to parameter FM and enter
  5. Connect the volt meter to terminals FM and CC
  6. Press the UP and DOWN arrows until meter reads desired 100% (10Vdc)
  7. Press enter to lock in the scale
  8. Set FMSL = 1 to follow motor current
ALL OTHER analog output functions (FMSL = 0,2,3 - 18)
4-20mA (no load)
  1. Set DIP switch FM (SW101) to "I" (left)
  2. Set F692 for 20 (20% of 20mA = 4mA)
  3. Set FMSL to 17
  4. Go to the FM parameter and enter
  5. Connect the current meter to terminals FM and CC
  6. Press the UP and DOWN arrows until meter reads desired 100% (20mA)
  7. Press enter to lock in the scale
  8. Set FMSL back to the analog output function you want to follow  per the table below.
​0-10Vdc (connect the load)
1. Set DIP switch FM (SW101) to "U" (right)
2. Set F692 to 0 (0% of 10V = 0V)
3. Set FMSL to 17 
4. Go to parameter FM and enter
5. Connect the meter between terminals FM and CC
6. Press the UP and DOWN arrows until meter reads desired 100% (10Vdc)
7. Press enter to lock in the scale
8. Set FMSL back to the analog output function you want to follow, per the table attached.

Note:  Calibration can also be performed using the VW3A1101 remote keypad.  Turn the knob clockwise instead of using the up arrow and turn counter clockwise instead of  using the down arrow.

 



 

Schneider Electric Saudi Arabia

Attachment(s)
FNSL.png [513.98 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: