{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the braking capacity of the ATV312HU15N4?
Issue:
Braking capacity ATV312HU15N4

Product Line:
ATV312

Environment:
All

Cause:
Braking capacity ATV312

Resolution:
Without a braking resistor, it is 50% of nominal motor torque. With braking resistor, it is 100% of motor torque continuous and 150% of torque for 60 seconds.

Schneider Electric Saudi Arabia