Search FAQs
How many IFMs can be stacked to an IFE Switchboard Server (LV434011)?
Issue:
End user would like to know how many IFM (Modbus Interface Modules) can be connected to a single IFE (Ethernet Interface) using the Stacking Connector
Product Line
IFE and IFM devices
Environment:
Modbus Communications
Cause:
It is possible to connect multiple IFM's to a single IFE
Resolution:
Twelve (12) IFMs can be stacked to an IFE Switchboard Server (LV434011) via the stacking connector. To find out more information about the stacking connecter please check out FA374688.
End user would like to know how many IFM (Modbus Interface Modules) can be connected to a single IFE (Ethernet Interface) using the Stacking Connector
Product Line
IFE and IFM devices
Environment:
Modbus Communications
Cause:
It is possible to connect multiple IFM's to a single IFE
Resolution:
Twelve (12) IFMs can be stacked to an IFE Switchboard Server (LV434011) via the stacking connector. To find out more information about the stacking connecter please check out FA374688.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: