{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Host Name field in NMC web interface returns with "has been entered incorrectly"
Issue
After trying to apply a host name in the web UI of an NMC, an error is returned saying "Host Name (XXXX) has been entered incorrectly." unless there is a "." in the name.

Product Line
Network Management Cards (NMC) - AP9630/AP9631/AP9635

Environment
All serial numbers
AOS v6.1.8

Cause
This was caused by an issue unique to AOS v6.1.8. It has been resolved in later firmware revisions.

Resolution:
Upgrade the firmware of the NMC to the latest revision

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.