{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we have a 230V single-phase input enclosed drive for a three-phase motor?
Issue:
230V single-phase input enclosed drive for a three-phase motor product selection

Product Line:
ATV61/71

Environment:
Irrigation Field Drive

Cause:
None

Resolution:
Schneider Electric provides a solution for single phase input, running a three phase motor with the Irrigation Field Drive.
Specific information can be found in the Altivar 61/71 Field Drive manual number 30072-454-01


Schneider Electric Saudi Arabia