{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the VW3A1101 keypad compatible with the ATV600 and ATV900 Series Process Drives?

Article available in these languages: Spanish

Issue:
VW3A1101 compatibility with the ATV600 and ATV900 Drives

Product Line:
ATV600 and ATV900 series

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
The VW3A1101 keypad is not compatible with the Altivar Process Drives. It is only compatible with ATV61, ATV71, ATV212, ATV312, and ATV32 Series Drives.

The keypad part number for ATV630 & ATV930 process drive is VW3A1111. An optional door mounting kit part number is VW3A1112.

Schneider Electric Saudi Arabia