Search FAQs
What is the reference for the separate mounting kit for LRD4369 overload relay
The LRD43xx type of thermal overload relays are directly mounted to the contactors LC1D115 & LC1D150 only. There is no separate mounting kit for the LRD43xx.
If a separate mounting is required for the contactors LC1D115 or LC1D150 type, then LRD336xx shall be selected as these range of overload relays have independent mounting and have similar setting ranges and are of Class 10A.
If a separate mounting is required for the contactors LC1D115 or LC1D150 type, then LRD336xx shall be selected as these range of overload relays have independent mounting and have similar setting ranges and are of Class 10A.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: