Search FAQs
What type of Communication Modules are available for the SEPAM Relays?
Product Line
SEPAM Communications
Environment
Networking and communications
Resolution
The protocols that are available are: DNP3, Modbus RTU, IEC 60870-5-103, Modbus TCP/IP, and IEC61850. Not all modules have the same type of protocols or type of communications. Attached is the communication accessory selection guide to help pick the correct module.
SEPAM Communications
Environment
Networking and communications
Resolution
The protocols that are available are: DNP3, Modbus RTU, IEC 60870-5-103, Modbus TCP/IP, and IEC61850. Not all modules have the same type of protocols or type of communications. Attached is the communication accessory selection guide to help pick the correct module.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: