{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you remove or uninstall an option card on the Altivar ATV61 and ATV71 Drives?
Issue:
Option card removal on the Altivar ATV61 and ATV71 Drives

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
Needs to uninstall or remove an serial communications or extended IO option card

Resolution:
Remove the front display cover by pushing down on the two tabs on the top of the drive.
Once the front cover has been removed you can now remove or uninstall your serial communications card or extended IO card by pushing in and down on the two tabs that are on top of the option card. Once the Option card has been removed you can not reinstall the front cover by pushing down on the cover until you hear it click into place.

Schneider Electric Saudi Arabia