{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you create and use a DTX file in Unity Pro?
Issue:
Creation and usage of the DTX file in Unity Pro

Product Line:
Unity Pro

Resolution:
The DTX file is a very useful tool that allows the user to capture the current values stored in %MW as well as unlocated variables. The data stored in the DTX file can be used to restore process data after an outage or capture tuning tuning values for start up. You can make any number of DTX files which would allow you to introduce different process recipes .

The following video will demonstrate how to create and use the DTX file.

Schneider Electric Saudi Arabia