Issue
Error message displayed when trying to delete a DTM
Potential issue due to the DTM version Compatibility"
"Warning: Potential issue due to the DTM version incompatibility. xxx DTM.
An error occurs during the check of DTM compatibility. DTM version in application is Vxxx).
DTM on the PC: not installed or installed without version information
Product Line
M580, BMENOC0301, BMENOC0311
Resolution
As of today, when a DTM is not installed, it is impossible to create the dynamic menu of the Dtm and then delete it.
We suggest to
Error message displayed when trying to delete a DTM
Potential issue due to the DTM version Compatibility"
"Warning: Potential issue due to the DTM version incompatibility. xxx DTM.
An error occurs during the check of DTM compatibility. DTM version in application is Vxxx).
DTM on the PC: not installed or installed without version information
Product Line
M580, BMENOC0301, BMENOC0311
Resolution
As of today, when a DTM is not installed, it is impossible to create the dynamic menu of the Dtm and then delete it.
We suggest to
- Install the required DTM
- DTM are vendor based and must be downloaded from the vendor website.
- Update the DTM catalog
- Open the application and the TOOL>DTM browser
- Delete the desired DTM from the DTM browser tree.
Released for:Schneider Electric Saudi Arabia