Search FAQs
PowerChute Serial Shutdown or PowerChute Business Edition will not discover Smart-UPS when using 940-0272A cable
Issue,
PowerChute Serial Shutdown or PowerChute Business Edition will not discover the Smart-UPS after connecting to Windows OS using the 940-0272A cable.
Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown
Environment:
All supported Windows OS
Smart-UPS
Cause:
To use the 940-0272A cable with PowerChute Serial Shutdown or PowerChute Business Edition, the Prolific USB to Serial driver must be installed before installing PowerChute.
Solution:
Download the latest Prolific PL2303 driver from http://www.prolific.com.tw/US/ShowProduct.aspx?p_id=225&pcid=41
For Windows Server Core/Hyper-V, the Prolific USB/Serial driver must be downloaded from the Windows Update Catalog onto the Windows Server Core/Hyper-V Server. The cab file must be extracted to local drive and pnputil -i -a ser2pl.inf must be run to install the driver. Windows systems with GUI need to have the Add New Device wizard check Window Update for the driver. Once the driver is installed, reboot the server to register the COM port in the OS.
PowerChute Serial Shutdown or PowerChute Business Edition will not discover the Smart-UPS after connecting to Windows OS using the 940-0272A cable.
Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown
Environment:
All supported Windows OS
Smart-UPS
Cause:
To use the 940-0272A cable with PowerChute Serial Shutdown or PowerChute Business Edition, the Prolific USB to Serial driver must be installed before installing PowerChute.
Solution:
Download the latest Prolific PL2303 driver from http://www.prolific.com.tw/US/ShowProduct.aspx?p_id=225&pcid=41
For Windows Server Core/Hyper-V, the Prolific USB/Serial driver must be downloaded from the Windows Update Catalog onto the Windows Server Core/Hyper-V Server. The cab file must be extracted to local drive and pnputil -i -a ser2pl.inf must be run to install the driver. Windows systems with GUI need to have the Add New Device wizard check Window Update for the driver. Once the driver is installed, reboot the server to register the COM port in the OS.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: