{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use SoMove software on a ATV28 drive (also ATV16, ATV18, ATV11, ATV56, ATV66)?
Issue:
Using SoMove software on a ATV28 drive (also ATV16, ATV18, ATV11, ATV56, ATV66).

Product line:
ATV28, ATV16, ATV18, ATV11, ATV56, ATV66

Environment:
SoMove

Cause:
n/a

Resolution:
No, SoMove will not work with ATV28 drives or any of these other, obsolete products.

We do not offer a software package for these old, discontinued and obsolete drives.

Schneider Electric Saudi Arabia

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: