{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to display a custom image for an object in a Vista diagram

Issue
A user would like to change the image displayed for a grouping, status, or control object in the Power Monitoring Expert Vista application.

Product Line

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
Diagram modifications in the Vista application.

Resolution
See Video below:

Schneider Electric Saudi Arabia