Issue:
Maximum number of drives to daisy chain
Product Line:
ATV32, ATV61 and ATV71
Environment:
Modbus TCP/IP
Daisy chain part number
ATV32 - VW3A3616
ATV71 or ATV61 - VW3A3310D
Cause:
None
Resolution:
The maximum number of devices is 32. However, there may be some limitations. Please see the attached.
Maximum number of drives to daisy chain
Product Line:
ATV32, ATV61 and ATV71
Environment:
Modbus TCP/IP
Daisy chain part number
ATV32 - VW3A3616
ATV71 or ATV61 - VW3A3310D
Cause:
None
Resolution:
The maximum number of devices is 32. However, there may be some limitations. Please see the attached.
Released for:Schneider Electric Saudi Arabia