Search FAQs
Are there status words available which will allow me to see module health on the Quantum ERIO network?
Yes, the following System Words will provide the health status of each IO module on the ERIO network.
%SW641-702 Referred to as ERIO Module Health. Refer to Control Expert Help for details which discuss how these words apply.
%SW641-702 Referred to as ERIO Module Health. Refer to Control Expert Help for details which discuss how these words apply.
16 bits of the word represent the 16 potential slots in a Quantum backplane.
0 = unhealthy or not mapped
1 = healthy module.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: