Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Will the new BMX redundant power supplies work with the M340?
The M340 will have the capability to use the redundant power supplies with the release of Unity V11.1 and using the BMEXBP backplanes. 
It does not mean the M340 will be able to communicate on the Ethernet link - M340 backplane communications will stay BusX only. The M340 
will also not have the ability to use the preventive maintanence library either. 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: