{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In Proworx 32 when I select"Controller/Read" will the complete program be transferred from PLC to PC?
Issue::   Uploading some or all of the project in the PLC.
Product Line: Prowrox 32

Answer: Yes the entire application program will be uploaded from the PLC to PC.
You also have the option to perform a Partial Upload which would allow
specific portions of the application to be transferred.  (Read / Read Extended Memory)


R-6-30-17

Schneider Electric Saudi Arabia