{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the total DC bus capacitance for the ATV960 drive in microfarads?

Issue:
Needs the total DC bus capacitance for the ATV960  in microfarads

Product Line:
ATV960

Environment:
All

Cause:
N/A

Resolution:
T
he DC capacitance for the ATV660/960 is 10mF per brick.

1p: ATV960C11 ... C16: 10mF
2p: ATV960C20 ... C31: 20mF
3p: ATV960C35 ... C50: 30mF
4p: ATV960C56 ... C63: 40mF
5p; ATV960C71 ... C80: 50mF

Schneider Electric Saudi Arabia