{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the communications cable between the Magelis XBTN200 / XBTN400 and Modicon M221 controller?
Issue:
What is the communication cable needed between an M221 and XBTN.

Product Line:
M221
XBTN200
XBTN400

Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.

Schneider Electric Saudi Arabia

Attachment(s)
XBTZ9980 pinout.jpg [25.74 KB]