{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between the Altivar 61/71 drives and the Altivar 61/71 Plus drives?

Issue:
Differences between the Altivar 61/71 drives and the Altivar 61/71 Plus drives.

Product Line:
ATV61/71 series

Environment:
All serial numbers for ATV61/71 series

Cause:
N/A

Resolution:
The Altvar 61/71 drives are open style IP20 rated drives meanwhile, the Plus drives are UL type 12 Enclosed drives that start at 125HP.
Please reference the attachment for additional information on the Altivar 61/71 Plus Drive series.

Schneider Electric Saudi Arabia

Attachment(s)

30072-454-96.pdf30072-454-96.pdf [5.74 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: