{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ENA (Pumpjack, Walking Beam pump) function available in the process drive?
ISSUE:
Availablity of ENA function (Pumpjack, Walking Beam Pump) in the Altivar Process Drives.

Product Line:
ATV600, ATV900 series

Environment:
All Models, All Serial Numbers

Cause:
Information unavailable in current literature.

Resolution:
The ENA function is not available in the ATV600 series process drives but is available in the ATV900 series process drives.
Please refer to the programming manual for the ATV900 series for further details.

Schneider Electric Saudi Arabia