Search FAQs
Can I use the service port on the M580 HSBY processor for SCADA traffic while servicing ERIO ?
Not recommended. Please consider using an NOC module. The service port does not support Rapid Spanning Tree Protocol and as a result the connection of each of these ports to a SCADA can result in an excessive amount of broadcast or ARP traffic.
We recommend using the NOC option module for SCADA in HSBY applications.
We recommend using the NOC option module for SCADA in HSBY applications.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: