Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure audible alarms as per different alarm priorities in Vijeo Citect?

Follow below mentioned steps to configure different audible alarms as per alarm priorities.

1. In Citect Project editor open Computer setup editor > under Alarm group add sound<n> parameter.  Browse and select the sound file (in .wav format) as per alarm priority.  Add sound<n>Interval in Ctect.ini. Same way different sound files can be configured as per different alarm priorities.

In Citect Project editor open Computer setup editor

2. Define alarm priority as per different alarm categories.

Define alarm priority as per different alarm categories.

3. Then go to Citect project Editor > Systems > Included Projects and add CSV_Include project.

dd CSV_Include project.

4. Run computer setup wizard and in the Events setup enable CSV_AlarmClient. Then complete the wizard and start runtime.

Run computer setup wizard and in the Events setup enable CSV_AlarmClient.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.