Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How to delete a DTM that was added with an EDS file from the library.
Issue
This resolution explains how to remove a DTM (added to the library through an import of an eds file) from the DTM library.

Product Line
Unity

Environment     
Windows 10

Resolution
Use the following steps to remove a DTM (added to the library through an import of an eds file) from the DTM library.
  • Open the DTM Browser.
bvcbb

 
  • Right click on the host IP address in the 'DTM Browser' window.
  • Select 'Add'
  • Select 'Device Menu'
  • Select 'Additional functions.
  • Select Remove 'EDS from library.'

vcvb

 
  • Click on the DTM name from the list on the 'EDS Delete from Device library.
  • Click on the 'Delete Selected Files' button.
vcb

 
  • Open the Hardware catalog.
vbvb

 
  • Click on the 'DTM Catalog' tab.
  • Click on 'Update'.

vcb

 
  • Click on Yes to confirm the update.
vcbb

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: