Issue
User is trying to purchase a cable to wire serial communication to EGX150 (Link150) to downstream devices through its RJ45 serial port
Product Line
EGX150 (Link150)
Environment
Serial communication
Resolution
Part# VW3A8306d30
This cable is for Modbus serial link 1xRJ45, free wires at the other end. 3m length
The correspondence between the wire colors of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:

User is trying to purchase a cable to wire serial communication to EGX150 (Link150) to downstream devices through its RJ45 serial port
Product Line
EGX150 (Link150)
Environment
Serial communication
Resolution
Part# VW3A8306d30
This cable is for Modbus serial link 1xRJ45, free wires at the other end. 3m length
The correspondence between the wire colors of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:
Released for:Schneider Electric Saudi Arabia