{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I detect the absence of input power or the loss of regulated output power of the BMXCPSxxxx ?
The BMXCPSxxxx has an onboard relay which the user can access. The relay is located on the front of the BMXCPSxxxx and will operate
as a N/C  (normally closed) contact when input and output power is within specification . Upon the loss of input voltage or if the output of the supply
falls out of specifications, the relay will open.





R-71317

Schneider Electric Saudi Arabia