A discrete input can be configured to the M580 from Run/Stop mode.
- Set %Ir.m.c to 1: The M580 switches to Run mode (execute the program).
- Set %lr.m.c to 0: The M580 switches to Stop mode (stop program execution).
NOTE: A Stop command takes priority over a Run command. A Stop command sent from a terminal or via the network has priority over the %lr.m.c input.An error detected on the Run/Stop input causes the M580 to switch to Stop mode.Do not activate this option if the associated discrete input is mapped in state RAM because this inhibits the start-up of the M580.
Managing Run/Stop Remote AccessWhen configuring the M580 CPU, you can help prevent remote commands/requests from accessing the CPU Run/Stop modes.
Select the respective Run/Stop input and Run/Stop by input only check boxes according to the following table parameters to
determine the type of remote access for your system.
Released for:Schneider Electric Saudi Arabia
A discrete input can be configured to the M580 from Run/Stop mode.
-
Set %Ir.m.c to 1: The M580 switches to Run mode (execute the program).
-
Set %lr.m.c to 0: The M580 switches to Stop mode (stop program execution).
NOTE: A Stop command takes priority over a Run command. A Stop command sent from a terminal or via the network has priority over the %lr.m.c input.An error detected on the Run/Stop input causes the M580 to switch to Stop mode.Do not activate this option if the associated discrete input is mapped in state RAM because this inhibits the start-up of the M580.
Managing Run/Stop Remote AccessWhen configuring the M580 CPU, you can help prevent remote commands/requests from accessing the CPU Run/Stop modes.
Select the respective Run/Stop input and Run/Stop by input only check boxes according to the following table parameters to
determine the type of remote access for your system.
Released for:Schneider Electric Saudi Arabia