{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If a NetShelter CX is scratched or dented can it be repaired? What color is the finish?
Issue:
A customer may want to touch up or repair damage to a NetShelter CX cabinet. 

Product Line:
NetShelter CX

Environment: 
All versions and serial ranges.

Cause: 
A NetShelter CX cabinet has been scratched or damaged. 

Resolution:
There are a couple of options a customer can use to disguise damage, but at closer inspection any repair work will remain visible. In most cases the repair will be visible. 
A color marker can help cover a scratch. To fill a hole or indentation it may be necessary to first fill it, then paint it. 
These are the colors that will patch: 
RAL - 7016
NCS - S8000-N
Pantone - 433U

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.