{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to replace email configurations in VIP using editor (Notepad or Notepad ++)
Issue

The customer has a massive VIP email alert module in their VIP to send out system alarms. The email configurations are saved in each module. When customer upgrade their email server or the email configuration has to be changed, it'll be time-consuming to change them in Designer. Notepad or free editor, Notepad++, can be used to search and replace email configurations. But simply replacing the value will make the VIP node not start

Product Line
Power Monitoring Expert (PME)

Environment

Virtual Processor

Cause

Here is an example of configuration:

value =
{
<21>ionalerts@company.com
}

Simply changing the text ionalerts@company.com with the desired email address such as PMEEmailAlert@company.com will not work, the reason is the number in the arrow bracket <#> should match the number of characters in the string. For example, ionalerts@company.com has 21 chars, and PMEEmailAlert@company.com has 25 chars,

Resolution

The replacement shall be:

Replace <21>ionalerts@company.com with <25>PMEEmailAlert@company.com

This principle applies to other configurations for the Email module.




Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: