{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The Write_Var instruction requires an Array of INT for the EMIS input. How do I move UINT values to a remote device?
You simply need to convert the UINT to INT with the UINT_TO_INT block and move the result to the EMIS array.
If the receiving device does not automatically see the data as UINT you would need to use the INT_TO_UINT block
to see the value correctly.

Schneider Electric Saudi Arabia