{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a parameter in the ATV32 that will allow me to reverse the output phase rotation?
Issue:
ATV32 parameter that will allow to reverse the output phase rotation

Product Line:
Altivar 32 series

Environment:
All models, All serial numbers

Cause:
Can not find a parameter to do this in current literature.

Resolution:
The ATV32 series drive does not have a means to reverse the output phase rotation via programming parameter. To reverse the direction of the motor, swap 2 leads on the output side of the drive. If you swap phase rotation on the input side of the ATV32, the motor direction will not change.

Schneider Electric Saudi Arabia