{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is an OCF trip code on the ATS22?
Issue:
ATS22 soft starter stopped running.  Display is showing OCF.

Product line:
ATS22, Altistart 22

Resolution:
OCF is caused by motor current that exceeds the OId (Overcurrent threshold) and OIt (overcurrent time delay) settings in the PrO menu.  The default settings for these from the factory are OId = 200% of the In setting and OIt is 0.5 seconds.

Check that the ATS22 is correctly setup for the application. In should be set at the motor FLA. UIn should be set to the measured Line voltage.  Check the setting of ILt under the SEt menu.

For example - if In is set for 100A, the Overcurrent fault would happen when the detected current reaches 200A for 0.5 seconds. OId can be increased to a maximum of 300% of the In value. OIt can be adjusted up to 5.0 seconds maximum.

This function is only active when the ATS22 is in rUn status.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia