{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME OPC tags have item quality "uncertainLastUsableValue"
Issue
Device communicates in PME successfully but reading OPC tags produces an error with a quality value of "uncertainLastUsableValue"

Product Line
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment
OPC

Cause
The tag being read is a custom measurement that does not have an entry in the IAS_MeasurementAddress table

Resolution
Mapping the measurement to a Data Recorder will force an entry into the IAS_MeasurementAddress table.
To do this:
1) Open Designer
2) Create a new Data Recorder
3) Link one of the inputs of the Data Recorder with the customer measurement that is not readable
4) Link an external pulse to the trigger of the Data Recorder so no actual data gets logged.

Once the measurement is mapped to the input of the Data Recorder, save the changes and close out of Designer.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: