Search FAQs
How to mount the hood of my ERDF Trunking system on Resi9?
To easily mount the ERDF cover, it is necessary to fix it on the outer wall of the trunking system and then close the separation on the inside.
An installation of flat cap with a fixation on the two sides at the same time is not recommended.
For more information please click:
https://www.se.com/ww/en/download/document/NVE6645101/
An installation of flat cap with a fixation on the two sides at the same time is not recommended.
For more information please click:
https://www.se.com/ww/en/download/document/NVE6645101/
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: