{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are fast screws sufficient to ensure the holding of the frame of my Resi9 Electrical Panel on Insulatin backpart?
Yes, the screws supplied with the chassis are sufficient (installed according to the description in the manual) if you are using the Plus backpart

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.