undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power monitoring Expert Vista "Unknown Command Line Argument" when run from command line

Issue
A customer is attempting to launch Vista through a command window but receives the following error message.
Unknown command line argument

Product Line

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment
Vista

Cause
The message indicates that when invoking the Vista executable only certain triggers are allowed.

Resolution
Each of the triggers below will launch Vista with that particular function.

1. -N refers to the name in the software table, typically VISTA.<machinename>
2. -U\-P are username\password - say supervisor\0.  This will allow Vista to launch without prompting for login credentials.
3. -I is for translation.  This switch loads the file named 'internat.txt' within \confg\internat and contains translated strings that the user can provide.  This will create a translated interface for that particular user even if it is different from the language package selected at installation.
4. -Geventviewer will launch Vista with a Global Event viewer.

You can add these arguments to a cmd line or shortcut, so the user does not have to authenticate and Vista will just start.

An example of using all triggers through a command prompt is below:

Administrator:  Command Prompt

This will launch Vista using the node name 'instance', the supervisor/0 login, with translation from the internat.txt file, and with a Global Event viewer.  In order for the Global Event viewer to display the 'Show Global Event Viewer' option under the View drop-down menu within Vista must be unchecked.  All triggers can be used in the same command or individually.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: