{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On the 8839EFD, with Hand Off Auto option, where do I connect the Auto Start contacts?
Issue:
Connection of Auto Start contacts on the 8839EFD with Hand Off Auto option.

Product Line:
8839 EFD

Environment:
Power Circuit with Hand-Off-Auto option

Cause:
Need for remote start

Resolution:
Auto Start contact should be installed on terminal block TB1 between pins 6 and 7.

Schneider Electric Saudi Arabia