{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find the System Monitor Server for Lita iPC?
With the new iPC offer:
- HMIPSOxxx
- HMIPEPxxx
- HMIBMUxxx
- HMIBMPxxx
- HMIPCCP2xxx
- HMIPCCU2xxx
we have the possibility to configure the System Monitor server on a 3rd party PC in order to monitor all Magelis iPC (Client/Agent) connected on the network.
To use this feature, you have to download and install the server module with the following link (SA30ServerSetup_Schneider.exe):
https://schneider-electric.box.com/s/3rek2wtque8lrvmb1ixgwivng7e6kmrl

Note: This file is not included in the restore DVD. By default, Server and Agent are already installed on the Magelis iPC.

Additional Information:
Remote Manage Devices Any Time, Any Where
System Monitor is a Console-Server-Agent web-based structure for cloud management. Agent
here refers to Box iPC devices, and server refers to the server directly in contact with the agent.
The server can be a physical entity located in a central control room, or a virtual host set up in a
cloud. Console refers to a web-based interface that connects to the server and communicates with
the agent through the server. Administrators can perform equipment status and maintenance
checks on System Monitor console through an Internet browser at any time, from anywhere, using
any connected device. The server-agent connection fit the MQTT communication protocol. This
improves connection security and stability, and also decreases development time for System
Monitor integration. The console-server-agent web-based structure not only lowers the difficulty
of setting up System Monitor network environments when provisioning, but also provides a
distributed connectivity structure that solves the challenges encountered with large-scale or multisite
device management. System Monitor is a real-time management platform that breaks
geographical limitations. Administrators can manage all of their devices by simply using their PCs,
smartphones, and tablets.

Please see the attached picture as example of structure.

Schneider Electric Saudi Arabia

Attachment(s)
System Monitor V3.0.PNG.png [158.81 KB]