{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the remote mount keypad for the ATV12 drives?

Article available in these languages: Spanish, Japanese

Issue:
Part number for remote mount keypad for the ATV12.

Product line:
ATV12, Altivar 12

Environment:
All serial numbers

Cause:
N/A

Resolution:
There are two keypad options: VW3A1006 (IP54) or the VW3A1007 (IP65).
The kit comes with the screws to mount the keypad to an enclosure or door.  A cable to connect the keypad to the drive is not included.  Customer needs to order cable VW3A1104R10 (1 meter) or VW3A1104R30 (3 meter) separately.



Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: