{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can a dry contact relay be programmed on the ATV212 drive to show Local/Remote status?
Issue:
ATV212 dry contact relay configuration to show Local/Remote status

Product Line:
Altivar 21 and ATV212 including the S-Flex enclosed drives.

Environment:
All

Cause:
Wants to monitor status to know when the drive is in local or remote.

Resolution:
Press Mode until you see AUF. Now arrow down to F--- hit enter.
Scroll up and find F130 or F132 depending on what relay you want to use.
F130 relay can be programmed for 56 Local remote status or 57 inversion of local rem status. RY RC contacts or F132 for FL relay same settings FLA FLC

Schneider Electric Saudi Arabia