{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider Electric offer motor type BDM4564S0115 ?
No, the motor type BDM4564S0115 is a customized version of Brushless DC motor which has special design features unique for the OEM machine builder that uses this model.

This model is proprietary for the OEM machine builder and the sale of this model is restricted to only the OEM.

Customers looking for BDM4564S0115 must contact the OEM machine builder to get spares.

rev 9-16-19

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: