{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can PM5300 data be accessed using a built-in webpage through its Ethernet port?

Issue
Can PM5300 data be accessed using a built-in web page?

Product Line
PM5300

Environment
HTTP server. Webpage access

Resolution
PM5300 does not have HTTP server and it does not have built-in webpages saved on its memory. Therefore, its data can't be accessed using this method.
The data is still accessible by reading Modbus registers through its Ethernet port.
PM5000 register list can be downloaded from FA234017

Schneider Electric Saudi Arabia